- Johnson Controls
- Building Insights
- Marine Visual Indicating Devices
Marine Visual Indicating Devices
Built on 100 Years of Product Innovation
The ZETTLER marine range has been built around MZX Technology, which provides some of the most advanced fire detection capabilities currently available. Developed by integrating many years of product innovation through research and development across Europe, the MZX Technology platform has provided some of the best sensing technologies over the last 100 years and has been a great contributor to early detection and in minimising false alarms. Our products have been designed to utilise tools and techniques that allow for easy and flexible engineering, configuration, and installation. It has also been responsible for some of the best installation techniques that allow for easy and flexible engineering and installation.
This has resulted in the ZETTLER range being one of the most resilient, reliable, and serviceable systems available with the broadest level of global standards compliance and certifications. With such heritage, ZETTLER experts have developed a new series of marine Visual Indication Devices (VIDs). When combined with our expert knowledge in fire detection technology and systems, this means that we now offer a range of superior devices that are among the most advanced available and that meet all the current standards and requirements.
Visual Indication Devices are generally used as a supplementary indication to raise situational awareness. But, when an event occurs, they cannot be used as the only means to alert people to a potential hazard.

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)