- Johnson Controls
- Marine and Navy
- ZETTLER Fire Detection
- Audio Visual Alarm Notification Solutions
Audio Visual Alarm Notification Solutions
Audio and visual notification is an advanced technology that’s helping take safety in a new direction
Ease of Use
From flexible wiring architecture to self-testing capabilities, our marine solutions are easy to use and cost-effective.Comprehensive
Our full suite of technologies can be tailored to meet a wide variety of marine and naval applications.Addressable
Addressable field devices promote easier implementation, testing, and maintenance.Benefits of notification
Additional benefits:
- Global addressability: Intelligent communications between initiating devices, notification appliances, and the control panel
- Fewer wires, more appliances per circuit, and fewer installation errors
- Appliances can be tested during installation for cost-efficient, on-the-spot problem resolution
- Enhanced survivability: Device-level ground faults are identified and isolated automatically
- Quick, unobtrusive testing of individual devices or an entire system
- Fast diagnostics and maintenance that lowers long-term cost of ownership
- All audio visual devices comply with EN54-23 in accordance with the needs of hearing impaired under the Equality Act 2010
How visual alarm devices enable effective lifesaving evacuation
In the event of a fire, saving lives is always the highest priority. Passengers and crew on a vessel need to be alerted as early as possible, using alarm devices, so they can leave or be evacuated. It is a mandatory requirement for sounders to be used as an integral part of the fire detection and alarm system, as they are considered the most important element of all alarm devices. Visual Alarm Devices are used to supplement sounders, providing an effective means of alerting, and evacuating people, as part of its fire safety strategy.
Learn more

Superior technology for the best protection
Johnson Controls experts have developed a new ground-breaking range of marine Visual Indication Devices (VIDs). When combined with our expert knowledge in fire detection technology and systems, this means that we now offer a range of superior devices that are among the most advanced available and that meet all the current standards and requirements.
Learn more