- Johnson Controls
- Media Center
- BlazeMaster CPVC offering: The Tyco Rapid Seal Sprinkler Head Adapter
Johnson Controls announces newest addition to its BlazeMaster CPVC offering: The Tyco Rapid Seal Sprinkler Head Adapter
UL, ULc, FM, NSF and LPCB approved, Rapid Seal contains no brass or lead
MILWAUKEE – (Feb. 5, 2018) – Johnson Controls announces the new Tyco® Rapid Seal CPVC Sprinkler Head Adapter. Made with BlazeMaster® CPVC compound for use in fire sprinkler systems to connect sprinkler heads to piping systems, Rapid Seal is easy to install and available in multiple sizes and styles.
With its all-CPVC design, Rapid Seal is less susceptible to dezincification in hard water environments, while also complying with growing state and federal low-lead requirements for sprinkler and plumbing systems. Further, its straight-thread adapter provides a more seamless, leak-free installation.
Additional benefits include its time-saving installation for contractors, as Rapid Seal has no thread tape or sealant, and its straight-thread design allows for flexible installation. This method provides a more precise positioning of the deflector, which is also ideal for the installation of horizontal sidewall sprinkler heads. Lastly, installation can be done by simply hand-tightening the sprinkler into place and finishing with a minor adjustment.
For more information about Tyco fire protection products, visit http://www.tyco-fire.com/. For questions or support, contact Tyco technical services at 1-800-381-9312.
About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco® , YORK® , Metasys® , Ruskin® , Titus® , Frick® , PENN® , Sabroe® , Simplex® and Grinnell® . For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
CONTACT:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com



















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)