- Johnson Controls
- Media Center
- New Tyco Series TY-B and TY-FRB Poly-Stainless Sprinklers
New Tyco Series TY-B and TY-FRB Poly-Stainless Sprinklers
Johnson Controls announces new Tyco® Series TY-B and TY-FRB Poly-Stainless Sprinklers
Corrosion-resistant sprinklers designed for use in commercial occupancies
MILWAUKEE – (Oct. 15, 2018) – Johnson Controls announces its new Tyco® Series TY-B and TY-FRB Poly-Stainless Sprinklers intended for commercial applications where corrosive conditions may exist. The TY-B has a 5 mm diameter heat-sensitive glass bulb rated standard response, while the TY-FRB has a 3 mm diameter heated-sensitive glass bulb rated quick response.
The corrosion-resistant Poly-Stainless Sprinklers are standard coverage sprinklers and available in in both upright and pendent orientations in either 5.6 or 8.0 K-factor.
All Poly-Stainless Sprinkler models have passed the standard corrosion tests of the applicable approval agencies; however, the effects of ambient temperature, concentration of chemicals and gas/chemical velocity should be considered, at a minimum, along with the corrosive nature of the chemical(s) to which the sprinklers will be exposed.
For more information, visit http://www.tyco-fire.com. For questions or support, contact technical services at 1-800-381-9312.
About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.
# # #
Photo Caption: The Tyco® Series TY-B and TY-FRB Poly-Stainless Sprinklers are designed for use where corrosive atmospheres can exist.
CONTACT
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com

















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)














.jpg?la=en&h=310&w=720&hash=8D9823F26AA80B2B75C3E4B2E61770DC)


.jpg?la=en&h=320&w=719&hash=13CA7E4AA3E453809B6726B561F2F4DD)
.jpg?la=en&h=306&w=720&hash=F21A7CD3C49EFBF4D41F00691D09AEAC)

.png?la=en&h=320&w=720&hash=18CFCCD916C92D922F600511FABD775D)