- Johnson Controls
- Media Center
- Tempmaster dedicated outside air systems
Tempmaster® dedicated outside air systems deliver more heating and cooling options to meet the demands of all climates and applications
Enhanced features meet advance requirements for fresh air and energy efficiency

The TempMaster® brand of Johnson Controls has released a new line of dedicated outside air systems (DOAS) to deliver flexible comfort options, enhanced indoor air quality and improved energy efficiency.
MILWAUKEE – (February 4, 2019) – The TempMaster® brand of Johnson Controls has released a new line of dedicated outside air systems (DOAS) to deliver flexible comfort options, enhanced indoor air quality and improved energy efficiency. A wide array of factory-installed options provides more combinations of heating and cooling than ever before including optional heat pump operation, water source operation and hot water heat options. The systems also feature an internal energy recovery wheel that pre-conditions 100 percent of outside air to reduce heating and cooling loads by transferring energy between the airstreams.
“Handling up to 18,000 cfm of air and providing as much as 70 tons of cooling capacity, the new Tempmaster DOAS meets ASHRAE requirements for building ventilation, provides efficient variable capacity compressors and addresses the needs of building owners and consulting engineers,” said John Tuleya, product manager, Applied DX products at Johnson Controls. “The dedicated outdoor air unit can control supply air to room neutral by utilizing multiple reheat options, provides superior control of high volumes of outside air while maintaining high indoor air quality.
“The dedicated outdoor air unit can control supply air to room neutral by utilizing multiple reheat options, provides superior control of high volumes of outside air while maintaining high indoor air quality."
— John Tuleya, product manager, Applied DX products at Johnson Controls
The new DOAS line offers air or water cooled units, in various configurations ranging from cooling-only to heat pump. A full selection of factory-installed options adds to system flexibility, including:
- Modulating or staged gas heat, SCR electric heat or hydronic heat options
- Six row evaporator coil for maximum capacity and moisture removal
- Multiple reheat options: modulating or on/off, liquid subcooling
- BAS connectivity
- Vertical or horizontal supply configurations
Often paired with another heating, and air-conditioning (HVAC) system, a Tempmaster DOAS can operate in conjunction with a separate sensible cooling system for a bundled solution. Paired system options include standard rooftop and self-contained units, chillers, water-source heat pumps, and variable refrigerant flow systems.
To learn more about TempMaster dedicated outside air systems, please visit www.TempMaster-HVAC.com
About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
# # #