- Johnson Controls
- Media Center
- Johnson Controls-Hitachi introduces Water Source Variable Refrigerant Flow systems
Johnson Controls-Hitachi introduces Water Source Variable Refrigerant Flow systems
Offer largest-capacity water source VRF systems in the industry, ranging from 6-48 tons

Johnson Controls-Hitachi Air Conditioning introduces the industry-leading Hitachi Water Source Variable Refrigerant Flow (VRF) systems.
MILWAUKEE – (September 3, 2019) – Johnson Controls-Hitachi Air Conditioning introduces the Hitachi Water Source Variable Refrigerant Flow (VRF) heat pump and heat recovery systems. The new multi-module systems offer the capability of connecting multiple single-module units, ranging from 6-48 tons. In addition to the benefits of VRF technology, these new compact systems deliver the following:
- Reduced first costs
- Compact size enhances exterior appearance while eliminating outdoor noise
- Design flexibility through a variety of configurations
- Ideal for projects with limited space such as high-rise buildings, office buildings, architecturally restricted properties and apartments
- Optimal where outdoor placement is challenging, including coastal areas and extremely cold climates
All Hitachi VRF indoor units, controls and gateway products are fully compatible with new water source systems for maximum design flexibility. The unified water source units can be used as heat pump and heat recovery units. They are available in 208/230V and 460V in 22 different capacities. Inverter compressor technology achieves high energy efficiency. The AHRI-certified efficiency ratings for the new Hitachi Water Source VRF systems include:
- Integrated Energy Efficiency Ratio (IEER) of 18.9 to 29
- Heating Coefficient of Performance (COP) of 4.00 to 6.30
For more information about the Hitachi Water Source VRF systems and other VRF products, please visit www.us.hitachiaircon.com.
About Johnson Controls
Johnson Controls is a global leader creating a safe, comfortable and sustainable world. Our 105,000 employees create intelligent buildings, efficient energy solutions and integrated infrastructure that work seamlessly together to deliver on the promise of smart cities and communities in 150 countries. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win everywhere, every day and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit http://www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable – one building at a time. Our technology portfolio integrates every aspect of a building – whether security systems, energy management, fire protection or HVACR – to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @johnsoncontrols on Twitter.
# # #