- Johnson Controls
- Media Center
- Envirco IsoClean portable HEPA filtration system
Envirco IsoClean® Portable HEPA Filtration System Creates Negative Pressure Isolation Environments
Ideal solution for occupants looking to minimize transmission risk in enclosed spaces

The IsoClean® HEPA Air Filtration system is an ideal solution for hospitals, nursing homes, and dorms hotels.
MILWAUKEE – (June 16, 2020) – Johnson Controls has introduced the Envirco IsoClean® filtration system designed to easily and economically create a negative pressure isolation room/environment that meets OSHA and CDC TB guidelines as the world navigates COVID-19 pandemic. IsoClean® can be used as a positive pressure clean air recirculating system in clinics, waiting rooms, hospital emergency rooms and other confined areas. The system can also be used as a partial or complete exhausting unit to construct a negative pressure isolation room space.
“The IsoClean® is an easy and economical solution that is ideal for health care professionals looking to create a negative pressure, isolation patient room,” said Mark Mattingly, vice president and general manager, Air Filtration Products, Johnson Controls. “The system can be easily rolled from one room to another and fits into areas with limited floor space. The portability and practical applications this solution offers is optimal for facilities looking for an economical investment.”
“The IsoClean® is an easy and economical solution that is ideal for health care professionals looking to create a negative pressure, isolation patient room.”
— Mark Mattingly, vice president and general manager, Air Filtration Products, Johnson Controls
Standard Features
Low cost isolation room: Simply roll the IsoClean® into a standard room, connect flexible ducting to the 6 in (152 mm) collar on the top of the unit for partial exhaust or to the optional 8 in. (204 mm) flanged collar for total exhaust and vent the purified air to the exterior through a window or wall.
Flexible applications: The versatile IsoClean® can be used as a clean air recirculating unit, a negative pressure unit or as a split system to create both negative pressure and clean air recirculation by simultaneously exhausting some of the air out while recirculating the remainder back into the room.
Hospital and other Applications
- Negative Pressure Rooms Emergency Rooms
- Waiting Rooms
- Sputum Induction
- Aerosol Pentamidine Treatment Intensive Care Units Bronchoscopy Rooms
- Renal Dialysis Rooms
- Clinics
- Nursing Centers
- Physician Offices
- Homeless Shelters
- Addiction Recovery Centers Correctional Facilities
To learn more about the IsoClean® visit: Kochfilter.com
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 105,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
# # #