- Johnson Controls
- Media Center
- YORK Mission Critical Horizontal Computer Room Air Handlers
YORK® Mission Critical Horizontal Computer Room Air Handlers Deliver Highly Efficient Cooling Performance and Scalability for Colocation and Hyperscale Data Centers

YORK Mission Critical Horizontal Computer Room Air Handlers (YORK MCH CRAH) from Johnson Controls are designed for hyperscale data centers.
- Purpose-driven design developed through close collaboration with demanding data center operators and key design and construction influencers
- Delivering on our customer’s challenges of reliability, OPEX efficiency, ease of use, serviceability and speed to market
- Backed by over 137+ years of industry experience, Data center customers know us best from our industry leading YORK chillers, Tyco fire & security solutions and service
MILWAUKEE – (September 21, 2020) – Johnson Controls today announced the YORK Mission Critical Horizontal Computer Room Air Handler (YORK MCH CRAH) designed to meet the unique cooling requirements of the world’s most demanding data centers. Offered in three standard capacities (105 kW, 210 kW and 315 kW rated at a 22F delta air temperature) with higher capacities available through customization, the YORK MCH CRAH is engineered with high-performance in mind and can be configured to meet the specific needs of each application.
With data hall space at a premium, Johnson Controls designed the YORK MCH CRAH for minimal footprint. The horizontal airflow unit features a compact (54”/1372 mm) length to save on equipment gallery floor space thus returning useable space to the IT data hall. Units feature left or right hand connections to minimize field piping, configurable chilled water coils and can be installed side-by-side with no gaps for optimal security, energy efficiency and space utilization for non-raised floor environments and facilities with heat containment strategies.
The YORK MCH unit incorporates a Johnson Controls flagship controller platform ensuring seamless integration to Johnson Controls Metasys or a 3rd party controls solution with support for all standard industry protocols.
The YORK MCH unit incorporates a Johnson Controls flagship controller platform ensuring seamless integration to Johnson Controls Metasys or a 3rd party controls solution with support for all standard industry protocols.
The MCH is designed for ease of use and with serviceability in mind. It has full-service access to fans, filters, electrical, coil and piping compartments on the gallery side minimizing the need for service technicians to access the secure data hall. Multiple finish options are available for the supply air outlet ensuring the aesthetics of the data hall.
“We developed the YORK MCH CRAH by collaborating with and listening to the current challenges of our customers and their design partners. We then harnessed the product teams at the York Airside Center of Excellence (ACE) and Johnson Controls Advanced Development Engineering Center (JADEC) to deliver a scalable solution that is perfectly suited for the most dynamic data centers,” said Brian Hatmaker, global director, Data Centers, Johnson Controls.
“With the introduction of the YORK MCH we are building on the remarkable air handling and mission critical tradition of the YORK brand. Data center customers know us best from our industry leading YORK chillers, Tyco fire & security solutions and HVAC equipment service. We are excited to extend these relationships into the data hall with the new YORK MCH product portfolio,” said Mike Zarrilli, director, Global Data Center Product & Ecosystem Lead.
The YORK MCH will be manufactured in dual locations, York, PA and Albany, MO, to ensure supply chain redundancy and strategic shipping points for delivery in North America.
Hatmaker adds, “Johnson Controls understands that speed to market is key for our colocation and hyperscale customers as they scale at incredible velocity. We bring value to those customers by engaging early and delivering specific solutions that enable project success. Our service organization then provides world-class support throughout the construction process and data center lifecycle.”
For more information, visit https://www.york.com/Commercial-Equipment/Air-Systems/Air-Handling-Units
Media Contact:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 105,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
# # #