- Johnson Controls
- Media Center
- Johnson Controls Launches Intelligent Frictionless Access Control for High Security Environments
Johnson Controls Launches Intelligent Frictionless Access Control for High Security Environments

Engineered with artificial intelligence, deep learning algorithms and robust cybersecurity protocols, the Tyco Illustra Insight solution is designed to create a frictionless, unobtrusive experience for all.
- Solution captures insightful, seamless movement of people in buildings, places and spaces
- Engineered with artificial intelligence, deep learning algorithms and robust cybersecurity protocols, the Tyco Illustra Insight solution is designed to create a frictionless, unobtrusive experience for all
- Integrated into OpenBlue, a dynamic platform for connected, safe and sustainable building solutions from Johnson Controls
MILWAUKEE - (Oct. 5, 2020) – Johnson Controls, the global leader for smart and sustainable buildings, has launched Tyco Illustra Insight, an intelligent frictionless access management solution for work environments where there is a requirement for a high level of security without disrupting the constant flow of employees, contractors and visitors. The solution offers an unobtrusive, stress free way for authorized people to smoothly move around buildings, places and spaces, and yet provides security personnel with a highly effective solution for controlling and visually verifying who has access to restricted areas.
Facial recognition
Enabled by artificial intelligence and deep learning algorithms, Tyco Illustra Insight combines the functionality of access control management software and a leading-edge facial recognition camera to simultaneously recognize multiple people as they approach an entrance. The device’s integrated LEDs, combined with audible ‘Welcome/Deny’ messaging ensure employees, contractors and visitors intuitively know if they are authorized to enter an area.
- Anti-spoofing technology utilizes two lenses and a combination of IR and RGB video to distinguish between an actual person and a printed image or video of them.
- Faces can be accurately detected from up to three meters away, with simultaneous multi-face processing in less than one second, improving the flow of approved users.
- The cameras can be deployed at the optimal height of five to six feet for facial recognition within a wide field of view and varying heights, including wheelchair and taller users.
"In healthcare and cleanroom environments, Tyco Illustra Insight removes the need for access control cards or buttons to be pushed, both of which are highly relevant to our customers amid the pandemic and beyond."
— Rafael Schrijvers, Access Control Product Management, Security Products, Johnson Controls
Versatile access management
“The range of applications where our new technology will be able to significantly contribute to enhancing a safer working environment is extremely wide and varied,” said Rafael Schrijvers, Access Control Product Management, Security Products, Johnson Controls. “In healthcare and cleanroom environments, Tyco Illustra Insight removes the need for access control cards or buttons to be pushed, both of which are highly relevant to our customers amid the pandemic and beyond.”
At airports it negates the risk of card sharing and tailgating into security sensitive areas. In addition to facial recognition, Illustra Insight can flag persons of interest for an integrated access control system to action; for instance, generating an alert when a VIP is identified.
Installers and system integrators will no doubt find many other imaginative ways in which this innovative combination of access control and video surveillance technologies, enabled by artificial intelligence, can deliver real-life benefits to their end-user clients.
Tyco Illustra Insight is part of the OpenBlue dynamic platform from Johnson Controls which, through its OpenBlue Healthy Buildings set of solutions, provides access to technology, such as smart equipment, infection control, contact tracing and social distance monitoring and other connected devices to make shared spaces safer, agile and more sustainable. OpenBlue was designed with agility, flexibility and scalability in mind to enable buildings to become dynamic spaces for customers that deliver environments that have memory, intelligence and unique identity.
Although designed for seamless integration with Johnson Controls access control brands, the Tyco Illustra Insight solution can also be interconnected to any access control system with on-board traditional and modern wiring protocols. Additional features include:
- Sleek form factor with full color customizable LED light ring and configurable audible messages maintain an inviting environment with intuitive visual and audible responses for visitors and employees.
- The unique two-piece design of Tyco Illustra Insight ensures that the network interface is in a safe, protected area, with encrypted protocols used to ensure secure communications between the Tyco Illustra Insight camera head and the Insight control unit.
- Tyco Illustra Insight has been engineered in line with the Johnson Controls OpenBlue Cyber Solutions Product Security Program, designed to minimize the possibility of introducing vulnerabilities into electronic security solutions.
Tyco Illustra Insight’s light ring and the option to record personalized greetings in a number of different languages are just two ways in which design engineers have endeavored to create a unique user experience which enhances the device’s ability to facilitate the free flow of people and set a new standard for automated video and access control.
To learn more, visit: http://www.illustracameras.com/insight
Media Contacts:
Ryan Nolan
Global Public Relations Program Manager
Building Technologies & Solutions, Johnson Controls
Work + 1 414 524 6170
Mobile + 1 414 378 9641
Ryan.P.Nolan@jci.com
Andrea Gural / Chelsie Woods
Eclipse Media Group on behalf of Johnson Controls
+1 207 233 7507 / +1 207 730 2396
agural@eclipsemediagroup.net / cwoods@eclipsemediagroup.net
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 105,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
###
Related Items
Access Control
Access control is the first line of defense when it comes to the security of your property. With a host of trusted brands in the industry, Johnson Controls offer an extensive range…