- Johnson Controls
- Media Center
- Tyco® DS-8 8.0K Dry Pendent Sprinkler for Outdoor Spaces and Commercial Freezers
Johnson Controls Introduces Tyco® DS-8 8.0K Dry Pendent Sprinkler for Outdoor Spaces and Commercial Freezers

Tyco DS-8 8.0K Dry Pendent Sprinkler
- Thermosensitive glass bulb can be used in sprinkler systems exposed to freezing temperatures
- 8.0 K-Factor and lower pressure provide additional design flexibility
- Suitable for wet, dry or pre-action sprinkler systems
MILWAUKEE – (January 12, 2020) – Johnson Controls, the global leader for safe, smart and sustainable buildings and architect of OpenBlue connected solutions, is expanding its Tyco DS Dry Sprinkler product family to include the DS-8 8.0K (K 115) Dry Pendent Sprinkler. The enhanced features of the DS-8 Sprinkler make it ideal for protecting commercial freezers and outdoor spaces like balconies, breezeways, loading docks and parking garages.
The DS-8 Dry Sprinkler provides more flexibility for designers and offers the possibility for lower design pressure compared to other dry sprinklers. It integrates seamlessly with the entire Tyco DS product portfolio, including the DSB-2 Dry Sprinkler Boot, to provide a single-source solution and ease of installation. The DS-8 is available in both quick response and standard response and is cULus Listed.
"With the addition of the DS-8, the Tyco DS portfolio represents the ultimate in dry sprinklers, both in function and finish."
— Bob Cordell, global product manager, Johnson Controls
“With the addition of the DS-8, the Tyco DS portfolio represents the ultimate in dry sprinklers, both in function and finish,” said Bob Cordell, global product manager, Johnson Controls. “The complete DS line supports our goal of enhancing building safety and increasing occupant satisfaction through innovative fire protection technology.”
The DS-8 Dry Pendent Sprinkler features a 3 mm or 5 mm thermosensitive glass bulb that can be used in cold environments, specifically in sprinkler systems that are exposed to freezing temperatures. With a variety of escutcheons (recessed, deep, standard or none), escutcheon finishes (including stainless steel) and custom piping lengths available, the DS-8 provides end users with the increased design flexibility and installation options to meet customers’ unique building project needs.
For more information about Tyco DS Dry Sprinklers from Johnson Controls, go to www.tyco-fire.com.
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 100,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
# # #