- Johnson Controls
- Media Center
- Johnson Controls Introduces Lithium-Ion Risk Prevention Solution
Johnson Controls Introduces Lithium-Ion Risk Prevention Solution for Protection of Energy Storage Systems

Lithium-Ion Risk Prevention System
- Designed to help protect Lithium-Ion Energy Storage Systems (ESS) in solar and wind farms, as well as Lithium-Ion batteries used in data centers and battery manufacturing facilities
- Provides rapid off-gas detection, battery stack disconnection and early intervention activation resulting in an integrated and comprehensive solution
- Delivers an early warning detection of off-gases and toxic vapors with a response time within a few seconds
MILWAUKEE – (February 18, 2021) – Johnson Controls, the global leader for smart, healthy and sustainable buildings, announces the launch of its Lithium-Ion Risk Prevention System. The system is engineered to provide early-warning detection of battery failure in Lithium-Ion Energy Storage Systems (ESS) and other applications using Lithium-Ion batteries such as UPS systems in data centers and manufacturing facilities. By monitoring and mitigating battery failure before it presents a fire threat, this technology provides immense safety value for the Energy Storage industry, which is rapidly growing due to global emission reduction targets in renewable power generation – particularly solar and wind.
The risk behind Lithium-Ion batteries
Lithium-Ion batteries provide a cost-effective energy storage solution for wind farms, solar farms and data centers. They can also pose severe risk if battery abuse occurs due to mechanical damage, charging failures, manufacturing defects or external heat. Battery abuse can result in thermal runaway – a dangerous chemical reaction within a battery cell that quickly spreads to adjacent cells. As it spreads, these cells collectively generate heat and smoke, which can potentially cause a fire event.
"The unique, three-step risk prevention system integrates off-gas monitoring and early intervention with traditional fire detection and suppression methods."
— Derek Sandahl, senior product manager, Johnson Controls
To help prevent catastrophic loss of assets, it is of paramount importance that battery cell malfunction is detected and mitigated prior to events that could lead to thermal runaway. This is best achieved by actively monitoring for Lithium-Ion off-gases, which are produced shortly after cell malfunction occurs.
Fully integrated early warning solution
The Johnson Controls Lithium-Ion Risk Prevention System features monitoring and reference sensors that continuously check battery racks for the presence of Lithium-Ion off-gases. The reference sensors provide surrounding ambient air data to the controller, while the monitoring sensors within the battery racks capture data relating to the air directly adjacent to the Lithium-Ion batteries. The sensors detect Lithium-Ion off-gases in a concentration as small as one part per million (ppm) and are compatible with all Lithium-Ion chemistries.
When the sensors detect off-gas, they immediately and automatically communicate with the battery management system to shut down the affected battery stacks to help prevent thermal runaway. In applications where the off-gases can build and cannot be vented externally, an inerting system may be employed to help prevent the off-gases from igniting. Early intervention helps protect valuable assets – extending the lifetime value of energy storage systems while keeping surrounding assets intact.
“The unique, three-step risk prevention system integrates off-gas monitoring and early intervention with traditional fire detection and suppression methods,” said Derek Sandahl, senior product manager, Johnson Controls. “The single system with monitoring can feed into a building management system, so all battery health information is provided quickly, and the system can respond appropriately.”
The Johnson Controls Lithium-Ion Risk Prevention System can be readily integrated into existing power storage systems since it does not require any electrical or mechanical contact with battery cells. For integration with fire detection and suppression systems, it is used with AUTOPULSE, ZETTLER or FIRECLASS Detection and INERGEN® or SAPPHIRE® Inerting or Fire Suppression Systems.
For more information on the Lithium-Ion Risk Prevention System, visit tycofpp.com/lithium-ion-RPS.
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 100,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, ANSUL® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.
# # #