- Johnson Controls
- Media Center
- YORK YVAM Magnetic Bearing Chiller
Johnson Controls maximizes data center cooling efficiency with new YORK® YVAM Magnetic Bearing Chiller

The YORK® YVAM air-cooled magnetic bearing centrifugal chiller is one of the most efficient options for data center applications.
- New magnetic bearing chiller lowers energy consumption and total cost of ownership
- Oil-free operation reduces routine maintenance needs
- Quick Start technology paired with integral uninterruptible power supply (UPS) backup allows it to power up to full load in approximately three minutes following a power interruption
MILWAUKEE — (May 18, 2023) — Johnson Controls, the global leader for smart, healthy and sustainable buildings, today announced the launch of the YORK® YVAM air-cooled magnetic bearing centrifugal chiller operating with the ultra-low global warming potential (GWP) refrigerant, R-1234ze, for hyperscale and colocation data center cooling.
The YORK® YVAM chiller is one of the most efficient options for data center applications, because its magnetic-bearing technology allows the system to operate very efficiently at low lift conditions. This means the chiller doesn’t need free cooling coils to deliver performance comparable to air-cooled chillers with integral water-side economizers. Compared to traditional air-cooled screw chillers, the YVAM can improve efficiency by 49% in non-standard part load value (NPLV) in typical data center conditions.
The pioneering design of the YORK® YVAM chiller was specified for the unique needs of mission critical applications, featuring industry-leading efficiency, simplified design and low harmonics,” said Chris Paraskevakos, vice president of product management, chillers and applied equipment, Johnson Controls. “Johnson Controls and the YORK® brand have a long history of serving the mission critical industry since 1998, and as such, owners and operators can have confidence in our equipment improving their operations, reducing the total cost of ownership and accelerating payback.”
The pioneering design of the YORK® YVAM chiller was specified for the unique needs of mission critical applications, featuring industry-leading efficiency, simplified design and low harmonics.
— Chris Paraskevakos, vice president of product management, chillers and applied equipment, Johnson Controls
The YORK® YVAM chiller uses a variable-speed drive with active front-end to lower energy consumption and total harmonic distortion. This means the magnetic driveline is significantly quieter than traditional air-cooled chiller drivelines that use screw compressors. Full-load sound is only 65 dBA at a distance of 10 meters. The machine’s lubrication-free design also eliminates the complexity of subsystems and reduces the costs of routine maintenance and system checks.
Data centers and other mission critical facilities require non-stop cooling. A power failure could jeopardize operations and lead to costly downtime and performance penalties. To maximize uptime, the YORK® YVAM features Quick Start technology with integral uninterruptible power supply (UPS) backup, allowing the chiller to return to full load in as little as three minutes after power is restored.
To learn more about the YORK® YVAM air-cooled magnetic bearing centrifugal chiller, visit: www.york.com/commercial-equipment/chilled-water-systems/air-cooled-chillers/yvam_ch/yvam-air-cooled-magnetic-bearing-centrifugal-chiller.
###
Media Contact:
Melissa Talbott
Manager, Public Relations, Global Products
Melissa.talbott@jci.com
About Johnson Controls
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.