- Johnson Controls
- Media Center
- FRICK FPHE-R units
Johnson Controls improves ease of installation and maintenance accessibility of new FRICK® FPHE-R units
- Upgrades to unit include larger access doors, reduced customer electrical penetrations, lower height and weight, and dirt-resistant exterior
- New units fit precisely onto footprint of previous Rooftop Freezer (RTF) units, requiring no adjustments when replacing former models
- Added roof membrane prevents moisture entrapment in building infrastructure
MILWAUKEE– June 1, 2023 – Johnson Controls, the global leader for smart, healthy and sustainable buildings, today introduced its new FRICK® Freezer Penthouse Evaporator-Retrofit (FPHE-R) model that includes design updates on proven technology to improve ease of installation and service for contractors while maintaining product efficiency.
“Our line of freezer evaporator units has been proven in the field for the past four decades, and we’ve heard our contractors’ input and advanced this product line to meet today’s industrial refrigeration challenges,” said Chris Paraskevakos, vice president, product management at Johnson Controls. “These new updates to the unit’s reliability and serviceability help provide a cost-effective solution for building owners. The product line will further expand in the next year.”
These new updates to the unit’s reliability and serviceability help provide a cost-effective solution for building owners.
— Chris Paraskevakos, vice president, product management at Johnson Controls
The new FPHE-R unit weighs less than its predecessor thanks to a lowered height, making it more cost-effective to purchase while allowing for easier shipment. A rerouting of the low-voltage junction box brings electrical access to the exterior of the unit, eliminating the need for electrical penetrations by the contractor. Larger service doors provide easier access for maintenance and service.
Additionally, a new exterior finish improves the aesthetics of these rooftop units and reduces adhesion of dust and dirt. An added single-layer rubber roof membrane creates a weatherproof seal between outside environmental conditions and roof seams, helping to prevent air and water infiltration that could cause ice build-up and other issues in the unit.
Meeting the needs of modern industrial refrigeration, these new units update the former FRICK® RTF product line. By maintaining the same footprint and duct openings, the FPHE-R can be installed as a drop-in replacement for previous RTF units without the need for new roof openings or curbs, making these ideal for retrofit applications.
The FPHE-R model is designed to sit on roof curbs open to cold rooms below. Building owners can choose from a variety of convenient options that come with this freezer evaporator, including factory-mounted and wired fan motor starters, removable cooling coil access panel in the enclosure, and more configurations. End users can log on to the FRICK® Coolware platform for a seamless experience in selecting the appropriate industrial refrigeration product for their application, including food and beverage and cold storage facilities.
To learn more about the FPHE-R model, please visit: https://industrialrefrigeration.johnsoncontrols.com/FPHE.
Media Contact:
Melissa Talbott
Manager, Public Relations & Media, Global Products
melissa.talbott@jci.com
###
About Johnson Controls
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.