- Johnson Controls
- Media Center
- New compact centrifugal heat pump by YORK
New compact centrifugal heat pump by YORK® delivers high-temperature water with superior efficiency
Now available in a smaller 400-ton capacity, the newly launched YORK® CYK heat pump fills a North American market gap by providing a practical, right-sized decarbonization solution for use in existing commercial building applications.

- The smaller 400-ton CYK heat pump model joins the existing 600 – 2,000-ton product line to extend application to more commercial facilities.
- Can reduce water and operational costs by as much as 50% when compared to traditional boiler and chiller applications.
MILWAUKEE – Dec. 12, 2023 – Johnson Controls, the global leader for smart, healthy and sustainable buildings, has re-engineered the industry-leading YORK® CYK Water-to-Water Compound Centrifugal Heat Pump to deliver superior operational savings and stringent sustainability standards. Now available in a smaller 400-ton capacity, the newly launched YORK® CYK heat pump fills a North American market gap by providing a practical, right-sized decarbonization solution for use in existing commercial building applications.
“As part of our ongoing commitment to sustainability, we have evaluated our legacy equipment roster to develop future-ready solutions that meet the rapidly evolving sustainability requirements faced by today’s building professionals,” said Todd Grabowski, vice president and general manager of Applied Equipment at Johnson Controls. “The CYK is a prime example of this innovation and supports the brand message of YORK applied equipment that ’We’re Not Waiting for the Future. We’re Engineering It.’ The base design surpasses ASHRAE 90.1 standards for energy efficiency and provides the flexibility to further enhance efficiencies based on the unique needs of each building.”
The YORK® CYK can reduce water and operational costs by as much as 50% when compared to traditional boiler and chiller applications. The YORK® CYK heat pump is available with optional ultra-low global warming potential (GWP) refrigerants, R-1234ze and R-515b, to further support decarbonization and net zero goals.
“As part of our ongoing commitment to sustainability, we have evaluated our legacy equipment roster to develop future-ready solutions that meet the rapidly evolving sustainability requirements faced by today’s building professionals."
– Todd Grabowski, vice president and general manager of Applied Equipment at Johnson Controls
Additionally, the heat pump delivers high-temperature hot water up to 170 degrees Fahrenheit by utilizing two electric motor-driven centrifugal compressors arranged in series. The design achieves simultaneous hot and chilled water cooling within the same equipment making it three-to-five-times more efficient than a traditional boiler and chiller combination. With the addition of an innovative double bundle condenser technology, the CYK can effectively manage unbalanced load conditions – high cooling load with low heating load – in a more compact footprint than alternative solutions.
In addition to reduced carbon emissions, the YORK® CYK heat pump delivers significant savings through reduced annual water and operational costs, and a streamlined installation process. The innovative design is compatible with existing high-temperature hot water heating systems, eliminating the need to replace air handlers and terminal heating devices, which is often required to accommodate the lower water temperatures associated with other heat pump products. When these benefits are combined, building professionals can expect a short-term payback on the equipment investment.
Additional YORK® CYK heat pump features include:
- Optional variable frequency drive further enhances performance and efficiency
- Energy-efficient turndown up to 30%
- Built-in capacity control for each compressor enables enhanced performance during off-design conditions
- Flexible design can be customized to reach hot water temperatures beyond 170 degrees Fahrenheit
The YORK® CYK heat pump is ideal for medium to large commercial buildings, university campuses, hospitals, industrial processes and district energy applications and can be used in new building or retrofit applications. For additional information visit https://www.york.com/commercial-equipment/chilled-water-systems/water-cooled-chillers/cyk_ch/cyk-water-to-water-compound-centrifugal-chiller-heat-pump.
Media Contact:
Kari Pfisterer
Director, Public Relations and Media, North America
kari.b.pfisterer@jci.com
###
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world’s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @JohnsonControls on social platforms.
Related Items
HVAC Equipment
Every facility needs climate control systems, and we offer the world’s largest portfolio of HVAC equipment and controls. Our solutions genera…