- Johnson Controls
- Media Center
- YORK introduces industry-first screw heat pump
YORK® Introduces Industry-first Screw Heat Pump Using Ultra-low gwp R- 1234ze Refrigerant while Achieving up to 4X Greater Efficiency
The YORK® YVWH Water-to-Water Dual Variable Speed Screw Heat Pump, the first screw heat pump in North America to use R-1234ze refrigerant.

Ideal for commercial and industrial facilities, the YORK® YVWH Water-to-Water Variable Speed Dual Screw Heat Pump is the first screw heat pump in North America to utilize ultra-low GWP refrigerant R-1234ze and delivers hot water up to 176° F
MILWAUKEE, Wisconsin, Jan., 15, 2024 – Johnson Controls (NYSE: JCI), the global leader for smart, healthy and sustainable buildings, today announced the launch of the YORK® YVWH Water-to-Water Dual Variable Speed Screw Heat Pump, the first screw heat pump in North America to use R-1234ze refrigerant. R-1234ze is a refrigerant with an ultra-low global warming potential (GWP) of 1, enabling the YVWH to go considerably beyond the refrigerant regulations that go into effect starting January 1, 2025, as currently proposed by the U.S. Environmental Protection Agency.
The YVWH is three times more energy efficient than a typical boiler and four times more efficient than traditional boiler and chiller equipment when providing heating, cooling and hot water for light commercial buildings and industrial processes. By replacing a boiler or traditional equipment with the YVWH heat pump, commercial and industrial facilities can significantly reduce their energy use, water consumption and carbon emissions while keeping occupants comfortable and processes running effectively.
“Low-GWP refrigerants and the electrification of heating and cooling with heat pumps are two essential pieces of a successful sustainability strategy.”
‒ Todd Grabowski, vice president and general manager of Applied Equipment at Johnson Controls
“Low-GWP refrigerants and the electrification of heating and cooling with heat pumps are two essential pieces of a successful sustainability strategy,” said Todd Grabowski, vice president and general manager of Applied Equipment at Johnson Controls. “Our teams engineered the YORK® YVWH heat pump to help our customers meet regulations and reach their net zero goals while satisfying their end-use applications. It’s another example of how we're engineering the future.”
With outstanding operational flexibility, the YVWH supports simultaneous heating and cooling functions and can be operated in three modes: heating only, cooling only or simultaneous heating and cooling. Especially advantageous for high-temperature hot water heating applications, the YWVH is the first screw heat pump that can provide water temperatures up to 176° F (80° C). At that temperature, the unit can provide 4,050 MBH of heating while simultaneously providing 200 tons of chilled water cooling at 41° F (5° C). The YVWH also features variable-speed drive and has excellent turndown that allows it to run with as low as 25% of the design-heating load.
Each YVWH unit is factory-tested to ensure performance and is highly scalable to meet application needs. Multiple units can be combined or work in parallel with other YORK water-to-water heat pumps like the CYK to increase capacity and application benefits.
The YVWH joins the YORK family of heat pumps, which serve applications ranging from small commercial buildings to district heating. YVWH product details can be found in the new Johnson Controls selection tool. Solution Navigator is a one-stop, real-time platform that speeds up and simplifies the building management process and makes it easy to find products that best meet application needs.
To learn more, about the YORK YVWH water-to-water screw heat pump visit: www.york.com/commercial-equipment/chilled-water-systems/commercial-heat-pumps/yvwh-200_ch/yvwh-200-water-to-water-variable-speed-dual-screw-heat-pump or search for “YVWH” in the Johnson Controls Solution Navigator.
MEDIA CONTACT:
Kari Pfisterer
Director, Public Relations and Media, North America
Email: kari.b.pfisterer@jci.com
###
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world’s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.