YORK® Launches 575 Volt, High-efficiency Air-to-Water Heat Pump

The YORK® YMAE 575 V Air-to-Water Inverter Scroll Modular Heat Pump is now available in a 575-volt compatibility for Canadian market.

A York 575 Volt, High-efficiency Air-to-Water Heat Pump

Share

  • YORK® YMAE has been redesigned with 575-volt compatibility to provide high-efficiency, decarbonized heating and cooling for Canadian market.
  • Heat Pump meets all Canadian Registration Number (CRN) requirements in most provinces.
  • YMAE 575 V is engineered to deliver decarbonized heating and cooling within a wide operating range and can achieve up to 60 F (140 F) water in low ambient conditions.


MILWAUKEE, April 29, 2024
– Johnson Controls, the global leader for smart, healthy and sustainable buildings, today announced the launch of the YORK® YMAE 575 V Air-to-Water Inverter Scroll Modular Heat Pump for use in Canada. The high-efficiency heat pump is now available in a 575-volt model, and is compliant with the Canadian Registration Number (CRN) requirements for pressurized equipment in certain provinces.

“The YORK® YMAE heat pump has achieved exceptional results around the world, and we are proud to further optimize its performance for the Canadian market,” said Gerald Laumann, global product manager, air-cooled scroll chillers and heat pumps, Johnson Controls. “Its high-efficiency design and use of low-GWP refrigerant makes it a smart solution to drive sustainability within a wide range of applications.”

“The YORK® YMAE heat pump has achieved exceptional results around the world, and we are proud to further optimize its performance for the Canadian market.”

– Gerald Laumann, global product manager, air-cooled scroll chillers and heat pumps, Johnson Controls

Building upon the award-winning YORK® Amichi™ platform, the YMAE 575 V features innovative, variable speed electronic vapor injection (EVI) scroll technology to significantly expand heating capacities. Available in two- and four-pipe configurations, the YMAE 575 V can deliver 60 C (140 F) water in heating capacities up to 443 MBH while in heating-only mode, and 546 MBH during simultaneous heating and cooling using recovered energy. The YMAE 575 V also utilizes the low-GWP refrigerant R-454B to help reduce emissions.

With a highly flexible, modular design, the YMAE 575 V provides an energy-efficient solution that is compatible with a wide range of applications including offices, schools, healthcare facilities and multi-unit residential buildings. This modularity simplifies installation and provides added design flexibility. Up to four modules can be factory-kitted to expand capacities while maintaining a minimal footprint.

The YORK® YMAE 575 V Air-to-Water Inverter Scroll Modular Heat Pump is part of the OpenBlue platform of connected equipment and is available on a short lead-time. Product details can be found in the Johnson Controls Solution Navigator, a one-stop platform that makes it easy to find products that best meet application needs.

To learn more about the YORK® YMAE air-to-water heat pump, visit www.york.com/commercial-equipment/chilled-water-systems/ymae_heat_pump_chiller_ch or search for “YMAE” in the Johnson Controls Solution Navigator.

Media Contact:

Melissa Talbott
Manager, Public Relations, Global Products
Melissa.talbott@jci.com

###

About Johnson Controls:

At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.

Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.

Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.

Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.

Share