- Johnson Controls
- Media Center
- Expanded Line of 90-150 Ton Commercial Rooftop Units
Johnson Controls Launches Expanded Line of 90-150 Ton Commercial Rooftop Units
New 90–150-ton YORK® Sun™ Premier commercial rooftop units drive sustainability, reduce operational costs and streamline maintenance.

- New 90–150-ton YORK® Sun™ Premier commercial rooftop units drive sustainability, reduce operational costs and streamline maintenance.
- With class-leading efficiency, it surpasses DOE requirements and CEE highest tier ratings.
MILWAUKEE, May 15, 2024 – Today, Johnson Controls, the global leader for smart, healthy and sustainable buildings, announced the expansion of the award-winning YORK® Sun™ Premier commercial rooftop unit (RTU) portfolio with new 90–150-ton units. Designed for office buildings, hospitals and schools, the Premier RTUs, reduces carbon emissions and drives sustainability while reducing operational and maintenance costs.
With a full portfolio ranging from 25-150 tons, the Premier RTUs exceed the Department of Energy (DOE) 2023 energy efficiency standards, and most available tonnages meet the stringent Consortium for Energy Efficiency (CEE) 2024 highest tier ratings. Offered in standard efficiency, high capacity or high efficiency, YORK® Sun™ Premier units can provide up to 31% greater efficiency at part-load than is required, depending on the standard.
“The expanded Premier line has been redesigned to deliver superior performance, efficiency and long-term value to customers."
— Sophia Bellos, vice president of product development, Ducted Systems, Johnson Controls
“The expanded Premier line has been redesigned to deliver superior performance, efficiency and long-term value to customers,” said Sophia Bellos, vice president of product development, Ducted Systems, Johnson Controls. “Now available from 25 to 150 tons, this wide tonnage range allows Johnson Controls to provide contractors with unmatched flexibility to meet the needs of a wide variety of applications.”
Available in two tiers of efficiency per tonnage, YORK® Sun™ Premier RTUs meet both stringent Department of Energy (DOE) 2023 energy efficiency standards and the Consortium for Energy Efficiency (CEE) highest tier ratings. They combine variable-speed compressor options, variable-speed drive fan options and low-GWP R-454B refrigerant with advanced airflow and heat transfer technologies to deliver a highly optimized system.
The feature-rich Premier systems maximize design flexibility by offering the broadest array of airflow features, including various airflow paths and duct configuration capabilities, meeting the needs across a variety of applications and building construction constraints. Features including airflow measurement stations, dirty filter gauges, filter pressure transducers and suction, liquid and discharge shutoff valves reduce time on the roof. At the same time, built-in redundancy of refrigeration circuits and variable frequency drives and twinning algorithms enhance reliability and uptime. They are Smart Equipment enabled to seamlessly connect to building automation systems such as Verasys™.
The 90–150-ton Premier RTUs are available from YORK®, Johnson Controls® and TempMaster® and are backed by a one-year parts warranty along with either a six- or one-year earned labor warranty (versus the industry-standard 30-day warranty). To learn more, visit: www.york.com/commercial-equipment/packaged-split-dx/packaged-rooftop-units/2550tpremier_ds/york-sun-premier-rooftop-units
Media Contact:
Melissa Talbott
Manager, Public Relations, Global Products
melissa.talbott@jci.com
###
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.
Related Items
HVAC Equipment
Johnson Controls' extensive portfolio of HVAC equipment and controls for efficient, reliable climate control in healthy buildings.
OpenBlue
Applying data from both inside buildings and beyond, our customers can now manage operations systemically.
Our Company
Johnson Controls is a world leader in smart buildings, creating safe, healthy and sustainable spaces.