- Johnson Controls
- Media Center
- Johnson Controls delivers Germany's first seawater heat pump
Johnson Controls delivers Germany's first seawater heat pump
The DualPAC heat pump, manufactured at Johnson Controls’ plant in Denmark, is at the heart of a pioneering project by the Neustadt municipality and is being funded by the Federal Ministry for Economic Affairs and Climate Protection.

First of its kind solution in Germany contributes to a sustainable energy transition
Ratingen, Germany, 24. Oct, 2024. Johnson Controls, the leader in smart, healthy and sustainable buildings, is supplying the municipality of Neustadt in Holstein, Germany, with a state-of-the-art heat pump that will use water from the Baltic Sea to generate green energy. The system will provide part of the heat supply to a new district in the city's harbor via its own heating network. This seawater solution is the first of its kind in Germany on this scale and represents a future model for the transformation of heat supply.
“Heat pumps are a crucial technology in the energy transition and provide an efficient and sustainable alternative to gas and oil heating,” said David Emin, General Manager for Johnson Controls, Germany. “Our cooperation with the Neustadt in Holstein municipality shows we can use the technology to harness one of the world’s most abundant and natural resources. We are proud to bring our expertise to this innovative project that is setting an example for carbon neutrality in Europe and beyond.”
Johnson Controls is providing its SABROE DualPAC heat pump — a two-stage heat pump that features a modular system to enable high temperature lifts — ideal for use in district heating applications. It uses sea water to generate a heating output of up to 700 kW. During the winter months when the water is colder, it will extract around 500 kW of heat from the water, which is raised to a higher temperature using electrical energy and then fed into the new district heating network. At peak times, it will be supplemented by heat from a nearby waste incineration plant and a heat storage facility.
Most of the world’s heating needs today are met with direct fossil fuel combustion. To decarbonize buildings and maintain a reliable grid, electrifying these systems with heat pumps is key.
The DualPAC heat pump, manufactured at Johnson Controls’ plant in Denmark, is at the heart of a pioneering project by the Neustadt municipality and is being funded by the Federal Ministry for Economic Affairs and Climate Protection.
"The seawater heat pump is the essential element of our climate-friendly heat supply concept," said Thomas Anthoni, project manager for heating at the Neustadt in Holstein municipal utility company. "With this solution, we are implementing a flagship project for the energy transition."
Most of the world’s heating needs today are met with direct fossil fuel combustion. To decarbonize buildings and maintain a reliable grid, electrifying these systems with heat pumps is key. They use one third of the energy of conventional heating systems and can generate three to eight times as much energy as they consume.
Johnson Controls was among the first providers of environmentally friendly heat pumps over 50 years ago and today offers one of the world’s most comprehensive range of heat pumps designed for a range of commercial, residential and industrial uses. The company provides solutions that lever-age a range of natural energy sources such as sea, river and lake water, wastewater, waste heat, solar, biomass, geothermal.
Johnson Controls recently expanded its manufacturing sites in Holme in Denmark, Izmir in Turkey, and Nantes in France, to meet growing heat pump demand in Europe, and continues to expand its portfolio to provide higher temperature heating at colder conditions, and across a wider range applications. Further customer references include Hamburg Energy, Energie Baden-Württemberg and Stadtwerke Rosenheim.
###
MEDIA CONTACT
Louise Colledge
+41 79 414 4996
louise.colledge@jci.com
Director, Public Relations and Media, EMEALA
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.