- Johnson Controls
- Media Center
- YORK® launches new Mission Critical Vertical Computer Room Air Handler for more sustainable data centers
YORK® launches new Mission Critical Vertical Computer Room Air Handler for more sustainable data centers
The YORK® Mission Critical Vertical Computer Room Air Handler is engineered to meet the growing demand for sustainable data center technology.
- Downflow air handling units are purpose-built to meet the demands of mission-critical data center applications.
- A small equipment size and flexible design offers unmatched versatility for above floor or under floor cooling.
- High-efficiency EC motors and plenum fans maximize PUE and enhance sustainability.
MILWAUKEE, October 23, 2024 – Johnson Controls (NYSE: JCI), the global leader for smart, healthy and sustainable buildings, today announced the launch of its new YORK® Mission Critical Vertical Computer Room Air Handler (MCV CRAH), engineered to meet the growing demand for sustainable data center technology.
Data centers are one of the fastest growing areas of new construction around the world. Ensuring they remain efficient and sustainable is critical. The new MCV CRAH is specifically designed to support rapid data center expansion while enabling highly efficient and sustainable energy use.
“HVAC equipment is responsible for as much as 40% of energy use within data center applications,” said Merle Brubaker, director of air handling systems, Johnson Controls. “Optimizing efficiency within these facilities is critical, but solutions must be flexible to keep pace with the industry’s rapidly changing landscape. The YORK® MCV CRAH was designed in close collaboration with data center operators to drive sustainability while meeting the unique requirements of data center facilities.”
“HVAC equipment is responsible for as much as 40% of energy use within data center applications. Optimizing efficiency within these facilities is critical, but solutions must be flexible to keep pace with the industry’s rapidly changing landscape."
Merle Brubaker, director of air handling systems, Johnson Controls
As the demand for data centers continues to surge, many building owners are turning to hyperscale and colocation growth options to minimize construction timelines and overcome land shortages. These new data centers often require specialized HVAC considerations for adequate cooling and effective energy management.
Featuring a vertical downflow and draw-through layout, the YORK® MCV CRAH is engineered to deliver reliable cooling in above-floor or under-floor data center applications. It has a compact footprint, multiple cooling capacities and true plug-and-play functionality. High-efficiency electronically commutated (EC) motors, plenum fans and low heat-dissipation cabinets also contribute to lower PUE values.
The YORK® MCV CRAH is available with multiple electrical options and 30kW-60kW power output to support phased data center expansion. Rapid manufacturing and simplified installation enable a fast and easy integration. An intuitive, touchscreen Human Machine Interface (HMI) streamlines operation by enabling operators and engineers to quickly and easily visualize and monitor setup, alarms and capacities. Gallery-side maintenance access to fans with integral slide out racks, filters and electrical backed by local expert support reduce risk and maximizes reliability and uptime.
YORK® Vertical CRAHs are manufactured on short lead times from dual laboratories within key North American locations to further enhance speed to market. To learn more about YORK® Mission Critical Vertical CRAHs, visit: www.york.com/commercial-equipment/industries/data-centers.
Media Contact:
Melissa Talbott
Manager, Public Relations, Global Products
Melissa.talbott@jci.com
###
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit www.johnsoncontrols.com for more information and follow @Johnson Controls on social platforms.