- Johnson Controls
- Media Center
- Johnson Controls announces investment in data centre liquid cooling company Accelsius
Johnson Controls Announces Investment in Data Centre Liquid Cooling Company Accelsius
CORK, Ireland, Oct. 6, 2025 /PRNewswire/ -- Johnson Controls, the leader in smart, healthy and sustainable buildings, today announced a multi-million dollar strategic investment in Accelsius, a leader in two-phase, direct-to-chip liquid cooling technology for data centres. Two-phase solutions use 'phase change' from liquid to vapor to remove heat, enabling more efficient heat extraction with reduced energy consumption.
Cooling is among the most critical equipment in a data centre, efficiently and reliably keeping the chips at the right temperature that are foundational to the digital economy and our everyday lives. However, with cooling systems accounting for 30% to 40% of a data centre's total energy, deploying energy- and water-efficient cooling solutions is one of the industry's most pressing challenges.
"With the sharp growth in AI, cooling innovation has become a front-line imperative to meet the increasing demands of high-density data centres," said Austin Domenici, vice president and general manager, Johnson Controls Global Data Centre Solutions. "Leveraging our leading capabilities, our mission is to drive the industry forward to unlock new levels of energy efficiency across the cooling chain."
"With power-dense AI workloads, data centres are moving to liquid cooling," said Josh Claman, CEO of Accelsius. "Our two-phase, direct-to-chip (D2C) cooling solutions use non-conductive fluids in highly efficient loops to stay ahead of the demanding power-dense AI and HPC workloads. This technology enables 35% OpEx savings over single-phase direct-to-chip and 8–17% total cost of ownership savings."
Johnson Controls has already pioneered a number of breakthrough innovations for data centres including its YORK® YVAM magnetic bearing chiller – a solution that consumes 40% less power annually as other available solutions with zero on-site water consumption, demonstrating how advanced technology can deliver sustainability and meaningful societal benefits. The technology was recently named to Fortune's "Change the World" list, and recognised as a data centre leader, top innovator and top leader by ABI Research. In addition, the company recently launched its Silent-Aire Coolant Distribution Unit (CDU) platform offering a wide range of scalable cooling capacities from 500kW to over 10MW in flexible designs that can meet the needs of any data centre. By adopting Johnson Controls' comprehensive thermal management solutions, owners and operators can significantly improve total facility efficiency, reducing non-IT energy consumption by more than 50% in most North American data centre hubs.
INVESTOR CONTACT: |
MEDIA CONTACT: |
Jim Lucas |
Louise Colledge |
Direct: +1 414.340.1752 |
+4179 414 4996 |
Email: jim.lucas@jci.com |
Email: louise.colledge@jci.com |
About Johnson Controls:
At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.
Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centres, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.
Today, Johnson Controls offers the world`s largest portfolio of building technology and software as well as service solutions from some of the most trusted names in the industry.
Visit johnsoncontrols.com for more information and follow @Johnsoncontrols on social platforms.
About Accelsius
Founded by Innventure, Inc. (NASDAQ:INV), Accelsius empowers data center and edge operators to achieve their business, financial and sustainability goals through advanced cooling solutions. The proprietary NeuCool platform provides best-in-class thermal efficiencies through a safe, two-phase liquid cooling system that scales from single racks to entire data centres. For more information, visit accelsius.com or follow us on LinkedIn.
SOURCE Johnson Controls International plc