How does Connected Fire Sprinkler work?

  1. Sensors continuously gather fire sprinkler system data such as pressure, temperature and water presence.
  2. The information is relayed to the customer dashboard via the Cloud.
  3. A proactive notification is sent to the customer identifying the time and location of the adverse condition. If the customer is off-site it is sent to their mobile device.
  4. The adverse condition is addressed before damage can occur – thereby avoiding costly system and building repairs.

Learn more about Connected Fire Sprinkler:Download sell sheet. Download infographic.