- Johnson Controls
- Metasys
Make modernization easy with Metasys
Now you can take the next step toward better building performance
The newest Metasys release expands access to its world-class user interface, offering clear modernization paths while enhancing UI and display capabilities. Additional cybersecurity safeguards help protect building systems, and new routers streamline integrations to maximize operator efficiency.
Get the Metasys interface on network engines
The world-class Metasys interface is now available on Metasys SNx series network engines, providing quick access to critical information. “Engine only” customers have a scalable path to upgrade the legacy Site Management Portal, which has entered restricted end-of-support. Gain the benefits of a user interface designed for the way building operators really work.
![A laptop screen displaying the Metasys interface alongside a Metasys controller overlaid on an image of high-rise buildings](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/laptop-screen-displaying-metasys.jpg?h=1037&w=1380&la=en&hash=0897192C31E2BB8EDF53C7FBFA565E31)
![A laptop screen displaying the new UI features of the Metasys interface alongside a Metasys controller](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/laptop-screen-displaying-ui.jpg?h=1037&w=1380&la=en&hash=2D1763A2553AFF64082C575BCED6F135)
Enhance operator efficiency with new UI features
Help increase operator productivity with these UI enhancements:
- Logic viewer clearly indicates command priority to reduce time spent troubleshooting
- Alarm notification bar shows pending alarms to speed troubleshooting and resolution
- Additional reporting and trend data supports performance improvements
Critical Environment Controller extends benefits
Bring better control of room pressure, air changes, temperature, and humidity to labs, healthcare settings and other critical environments with the Metasys Critical Environment Controller. Faster input refresh rates and PID loops enable this next-generation controller to respond quicker to airflow changes like fume hood sash movement and door openings.
- BACnet MS/TP controller that responds to environment changes in milliseconds
- Multiple input and output configuration options with available expansion pack
- Runs pre-engineered and user-programmed applications
- Programmable with the Controller Configuration Tool (CCT)
- Comes valve-mounted, panel mounted or standalone
![A Metasys Critical Environment Controller overlaid on an image of an operation theatre](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/metasys-critical-environment-controller.jpg?h=1037&w=1380&la=en&hash=63CDFBE05F2A600C671EA15C2C36D5C7)
![Router and gateway devices overlaid on an image of high-rise buildings](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/router-and-gateway.jpg?h=1037&w=1380&la=en&hash=7F06D8D2BA6AD54C2848180F693C1416)
Streamline integrations with universal router and gateway
A new BACnet/IP router and Modbus gateway streamline integrations and reduce costs. Benefits include:
- Integration of third-party Modbus equipment into the BAS
- Support for up to 100 devices
- No need for a dedicated Metasys engine
Improve field productivity
Local controller, CG controller and network engine display models offer new features including plug-and-play functionality—out-of-the-box displays require no configuration.
![Metasys controllers and network engine display models overlaid on an image of a high-rise building](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/metasys-controllers.jpg?h=1037&w=1380&la=en&hash=7279163381B6A03D43A1256CC7463CFD)
![Five Metasys wireless system devices against a blue background](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/five-metasys.jpg?h=1037&w=1380&la=en&hash=99E429A0A2D71D351A105AC900275332)
Metasys wireless system delivers maximum performance
The WRG1830/ZFR183x Pro Series Wireless Field Bus System helps optimize flexibility, control and comfort while saving time and money. Explore the overview brochure, then reach out to our team to see how it can work for you.
CONTACT US
Additional options to complement Metasys
Build out your BAS with products you can trust. Choose the components you know will deliver essential data to Metasys, enhancing controls to achieve healthy building, net zero and bottom-line goals.
Valves & Actuators
Get the right temperature, pressure and flow solutions to create a truly dynamic building system.
Sensors
Powerfully precise HVAC sensors deliver cost savings in wireless networked, networked and non-networked solutions.
Thermostats
Make comfort and control convenient and cost-effective with a full range of commercial and residential thermostats.
![Icon depicting network engines](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/metasys-snesseries-network-devices-iconv.png?h=324&w=576&la=en&hash=008EAB4B2486B8DF9B1BBFF0E7967D12)
Powerful SNE Series Network Engines
Next-generation network engines pack high-capacity memory, fast processing, and advanced security features in a compact design. Enhance performance and reduce installation costs.
![Icon depicting Award-winning dashboard](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/laptop-award-pin-iconv.png?h=324&w=576&la=en&hash=AEE26BC4D3DFC3BD16868526CFE2116D)
Award-winning Cyber Health Dashboard
Alerts help you identify out-of-date software, policies, and permissions so you can address potential concerns.
![Icon depicting an open laptop](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/open-laptop-palace-circle-iconv.png?h=324&w=576&la=en&hash=15E64D2E3AC98F77265C01BCE0B4F322)
Open Application Server, open API
Our high-value OAS combines Metasys server and engine capabilities, bringing world-class user interface benefits to conventional controls. Our open API simplifies third-party integrations, furthering our commitment to openness.
![Collage of two images depicting building automation systems.](/-/media/project/jci-global/johnson-controls/us-region/united-states-johnson-controls/campaigns/metasys/lifestyle-images/collage-of-two-images.jpg?h=800&w=784&la=en&hash=CA04DE29CCCE0844AADE750B8FFAE505)
You can’t afford an out-of-date BAS
Metasys is designed for the way you work today, with built-in features to reduce risk, help your building perform better, and make your job easier. Let us take you to the next level.
SEE REASONS TO MODERNIZETake the next step toward better building performance. Contact us today.
Complete the form below to get in touch with our Metasys experts. We’re eager to show you the latest features and enhancements.
Metasys in the news
The role of building automation systems has never been more important. See what experts have to say about current trends—and Metasys benefits.
CONTROLTRENDS: The Future of Building Automation Controls
Bill Schwebel, VP & General Manager of BAS & Controls, Global Products, discusses the Johnson Controls journey and how it has set the stage to become the leading building technology company in the world.
FACILITY EXECUTIVE: CCM09090 Controller Provides Optimal IAQ
Detailed overview describes what you need to know about this room-level controller for healthcare facilities and complex labs—including the CCM09090’s faster response rate to changes in pressure.
ACHR NEWS: Keys to Success in HVACR Automation
Where to start to benefit from state-of-the-art systems like Metasys? Experts say to focus on education, collaboration and coordination.