Missouri University of Science and Technology
Upgrading to connected chillers to deliver data-driven performance
When one HVAC asset can affect them all, increasing uptime is mission critical. The campus of Missouri University of Science and Technology (Missouri S&T) is comprised of over 100 buildings, half of which are connected via a chilled water loop system and geothermal plant.
The interconnected nature of this system means one building’s chiller asset can have a profound effect on all 49 other facilities in the loop. As a result, when it came time to replace a chiller within the electrical engineering building, the university’s facilities team wanted to invest in a solution that would improve uptime and efficiency.
Learn more about the work we do
Related Items
Metasys 12.0
The newest Metasys release helps enhance security with BACnet/SC compliance, speeds troubleshooting, and maximizes system performance.
HVAC Equipment
Johnson Controls' extensive portfolio of HVAC equipment and controls for efficient, reliable climate control in healthy buildings.



















.jpg?la=en&h=320&w=720&hash=244C75B74F0F77521D56164450973BCD)