ANSUL® acoustic nozzle receives UL verification

An ANSUL® Acoustic Nozzle with its Underwriters Laboratories (UL) Verification

Share

Date 05/10/2018

MILWAUKEE - (May 10, 2018) - Johnson Controls recently received Underwriters Laboratories (UL) Verification for its ANSUL® Acoustic Nozzle, making it the first fire protection product to earn a marketing claim verification for performance. This independent, science-based assessment confirms the accuracy of a manufacturer's marketing claims, allowing customers to be confident in their product selection.

The acoustic nozzle earned the verification for this claim: "1/3 octave sound power is less than 110 dB for regulated flow and less than 113 dB for orifice flow." UL will present the verification certificate to Johnson Controls at the National Fire Protection Association Expo, June 11-14 in Las Vegas.

"We are pleased to award Johnson Controls the first industry UL Verification for acoustic nozzle performance," said Ghanem Zureikat, UL global business development manager. "This objective, third-party validation allows companies to stand out from those with self-declared or unsubstantiated claims."

The ANSUL Acoustic Nozzle, in combination with the INERGEN Fire Suppression System, is particularly useful for suppressing fires in hazards where sound levels may affect sensitive electronic equipment. The ANSUL Acoustic Nozzle passed all UL testing standards to perform as acoustically intended using exclusive sound power calculation software.

"It's exciting to have the first UL Verified claim in the fire protection industry," said Derek Sandahl, global product manager, engineered fire suppression systems at Johnson Controls. "The UL Verification Mark provides confidence to our customers in the stated acoustic performance of our Suppression System Acoustic Nozzle."

The ANSUL Acoustic Nozzle directs agent into the hazard area and reduces the sound level compared with standard nozzles. Flow calculations are used to specify the nozzle orifice size for the correct quantity and distribution of agent. This game-changing product is UL Listed with INERGEN 150, 200 and 300-bar fire suppression systems and replaces the standard INERGEN nozzle without major pipe rework or hydraulic adjustments, making it an affordable solution for retrofits.

About Johnson Controls
Johnson Controls is a global diversified technology and multi-industrial leader serving a wide range of customers in more than 150 countries. Our 120,000 employees create intelligent buildings, efficient energy solutions, integrated infrastructure and next generation transportation systems that work seamlessly together to deliver on the promise of smart cities and communities. Our commitment to sustainability dates back to our roots in 1885, with the invention of the first electric room thermostat. We are committed to helping our customers win and creating greater value for all of our stakeholders through strategic focus on our buildings and energy growth platforms. For additional information, please visit www.ansul.com.

About Johnson Controls Building Technologies & Solutions
Johnson Controls Building Technologies & Solutions is making the world safer, smarter and more sustainable - one building at a time. Our technology portfolio integrates every aspect of a building - whether security systems, energy management, fire protection or HVACR - to ensure that we exceed customer expectations at all times. We operate in more than 150 countries through our unmatched network of branches and distribution channels, helping building owners, operators, engineers and contractors enhance the full lifecycle of any facility. Our arsenal of brands includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, PENN®, Sabroe®, Simplex® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow @JCI_Buildings on Twitter.

Share