- Johnson Controls
- Media Center
- YORK® expands line of premium rooftop units to 60-80 tons
YORK® Expands Line of Premium Rooftop Units to 60-80 Tons with Faster Installation and Start-up
- Newly expanded YORK® Sun™ Premier rooftop unit line delivers simplified service with new digital features, such as an optional high-end graphical user interface
- Start-up is streamlined to offer best-in-class energy efficiency and significant reduction of operational costs with the new RTUToolkit app
- Seamless integration with Johnson Controls OpenBlue digital platform
MILWAUKEE – (March 9, 2021) – Johnson Controls, the global leader for smart, healthy and sustainable buildings, has, through its YORK® brand, expanded its line of premium commercial rooftop units now available in 25-80 tons with new, dynamic features. The expanded YORK® Sun™ Premier platform is designed to offer contractors faster installation and simplified start-up, while providing building owners with best-in-class efficiency levels that significantly reduce operational costs over the life of the unit.
"The expanded Premier line gives our customers additional features to ensure efficient start-up and installation so contractors can finish their jobs faster, while providing unmatched efficiency and reliability in the long term."
— Kevin Stockton, senior product manager, Johnson Controls
“YORK is committed to creating industry-leading equipment designed for performance, confidence and long-term value to customers,” said Kevin Stockton, senior product manager, Johnson Controls. “The expanded Premier line gives our customers additional features to ensure efficient start-up and installation so contractors can finish their jobs faster, while providing unmatched efficiency and reliability in the long term.”
To simplify system configuration and minimize start-up time, units feature start-up wizards, a 5.5-inch OLED display and an optimized numeric keypad, which are standard on all units. This can be upgraded to the optional new high-end graphical user interface, which features a full-color touchscreen that provides quick access to system status, performance metrics and schedule parameters. Start-up is further simplified with the new RTUToolkit app for Android and iOS. With the app, contractors simply scan a unique QR code on each rooftop, which enables on-demand access to unit-specific details, technical literature and direct connection to technical support.
Premier rooftop units streamline the design process with integrated system selection tools, easily accessible building information modeling files, improved submittals and simplified specification. The high-performance base models offer a complete range of factory options. These include various airflow path configurations, indoor environmental quality options, such as ultraviolet lights, and modulating options for improved comfort.
Maintenance is also simplified with service-friendly features, such as an optional Mobile Access Portal gateway that offers remote monitoring for ease of connection while at the jobsite, allowing technicians to interface with units without getting out of the truck. In addition, the Smart Equipment-enabled units provide seamless integration with leading building controls systems, including Verasys, and with OpenBlue, a dynamic connected platform for smart, healthy and sustainable building solutions from Johnson Controls.
YORK® Sun™ Premier commercial rooftop units meet aggressive Department of Energy 2023 energy efficiency standards. Offered in standard efficiency (up to 10.9 EER/15.8 IEER), high capacity or high efficiency (up to 11.4 EER/16.9 IEER), Premier units can provide up to 50 percent greater efficiency at part-load than is required, depending on the standard. Modulating options, such as compressors, an energy recovery wheel and gas or electric heat, further improve energy efficiency.
Premier units are backed by industry-leading warranties, offering greater peace of mind. A one-year parts warranty is standard on all Premier units, along with either a six-month or one-year promotional labor warranty (vs. the industry-standard, 30-day labor warranty) when started by a certified contractor. For more information about the Premier rooftop units, visit: www.york.com/sunpremier
###
About Johnson Controls
At Johnson Controls, we transform the environments where people live, work, learn and play. From optimizing building performance to improving safety and enhancing comfort, we drive the outcomes that matter most. We deliver our promise in industries such as healthcare, education, data centers and manufacturing. With a global team of 100,000 experts in more than 150 countries and over 130 years of innovation, we are the power behind our customers’ mission. Our leading portfolio of building technology and solutions includes some of the most trusted names in the industry, such as Tyco®, YORK®, Metasys®, Ruskin®, Titus®, Frick®, Penn®, Sabroe®, Simplex®, Ansul® and Grinnell®. For more information, visit www.johnsoncontrols.com or follow us @johnsoncontrols on Twitter.