ANSUL® R-102 Restaurant Fire Suppression System Receives EN 17446 Certification

The ANSUL R-102 Restaurant Fire Suppression System is now certified to EN 17446 standards.

A collection of ANSUL R-102 Restaurant Fire Suppression System units

Share

EN 17446 is the first common testing standard of its kind across Europe

MILWAUKEE, Wis., April 17, 2024 – Johnson Controls is proud to announce that the ANSUL R-102 Restaurant Fire Suppression System is now certified to EN 17446 standards by BSI, the business improvement and standards company (Kitemark 804125). The new certification further solidifies the system’s reputation as a trusted and reliable solution for safeguarding food service kitchens against the devastating impact of restaurant fires around the world.

The R-102 system already complies with EN 16282-7, which was published in 2017 and standardized practice across Europe by creating consistent hazard classifications, performance testing, and service and maintenance guidelines related to the installation and use of fixed fire extinguishing systems.

“This recognition demonstrates our commitment to delivering innovative fire suppression solutions around the world that meet the highest international standards and help make commercial kitchens safer.”

— Jan Waldow, business development manager at Johnson Controls

The new EN 17446 standard describes the testing requirements in detail for multiple appliances with different risk factors. To receive EN 17446 certification, the R-102 system was vigorously tested across a wide range of commercial appliances like griddles and cooktops that are known to be grease-vapor-producing. The system is able to protect:

  • Ranges up to 762 mm deep
  • Griddles up to 762 mm deep
  • Fryers up to 705 mm deep
  • Tilt skillets up to 705 mm deep
  • Gas radiant broilers up to 914 mm deep
  • Electric broilers up to 863 mm deep
  • Ducts and plenums of multiple sizes

Appliances larger than those listed above may be covered using multiple nozzle protection. See the R-102 Restaurant Fire Suppression System manual for additional details.

“The testing regime required to meet EN 17446 offers a significant and necessary challenge to ensure compliance, and I would expect that only the most robust systems will be able to meet these requirements,” said Jan Waldow, business development manager at Johnson Controls.

Jan Waldow is an industry expert who represented the German standards body (DIN) during the development of the EN 17446 standard.

Jan concluded, “This recognition demonstrates our commitment to delivering innovative fire suppression solutions around the world that meet the highest international standards and help make commercial kitchens safer.”

Complying with kitchen fire safety testing standards

Commercial kitchens in restaurants and hotels can be particularly vulnerable to fires, which are potentially harmful not only to health and safety but also to business operations. According to the NFPA, three out of five fires (61%) in eating and drinking establishments involve cooking equipment with deep fryers being the main culprit.

Such statistics emphasize the need for commercial kitchens to put clear safeguards in place for the safety and well-being of people and operations. Independently tested systems like R-102 that comply with the latest standards and are proven to extinguish fires quickly should maintain preference with restaurant specifiers, operators and insurers alike for safer fire protection, added reliability and peace of mind.

For added reassurance, ANSUL-certified technicians carry identification cards that show they have completed all relevant training for design, installation, commissioning, recharge, service and maintenance of both retrofits and new fire suppression systems.

Visit firesuppression.johnsoncontrols.com/Ansul_EN-17446 to see testing videos of the ANSUL R-102 Restaurant Fire Suppression System and learn more about how it complies with the EN 17446 standard.

Media Contact:
Melissa Talbott
Manager, Public Relations, Global Products
Johnson Controls
melissa.talbott@jci.com
414 307 0197

###

About Johnson Controls

At Johnson Controls (NYSE:JCI), we transform the environments where people live, work, learn and play. As the global leader in smart, healthy and sustainable buildings, our mission is to reimagine the performance of buildings to serve people, places and the planet.

Building on a proud history of nearly 140 years of innovation, we deliver the blueprint of the future for industries such as healthcare, schools, data centers, airports, stadiums, manufacturing and beyond through OpenBlue, our comprehensive digital offering.

Today, with a global team of 100,000 experts in more than 150 countries, Johnson Controls offers the world’s largest portfolio of building technology and software, as well as service solutions from some of the most trusted names in the industry.

Visit www.johnsoncontrols.com for more information, and follow @JohnsonControls on social platforms.

About ANSUL

ANSUL is the premium fire suppression product brand of Tyco International (U.S.), Ltd. The full line of ANSUL special hazard fire protection products include fire extinguishers and hand line units; pre-engineered restaurant, vehicles and industrial systems; sophisticated fire detection/suppression systems; and a complete line of dry chemical, foam and gaseous extinguishing agents. ANSUL products are developed and tested at the ANSUL Fire Technology Center, one of the most extensive fire research and testing facilities in the world. ANSUL products meet the demanding challenge of industry and commerce, including high-hazard/high-risk markets such as automotive, aviation, mining, chemical and petrochemical, utility, fire service and metal manufacturing/processing industries. For more information, visit www.ansul.com.

Share

Related Items

Exterior of a commercial building with glass windows

Fire Suppression

From sprinkler systems to water mist installations, we provide commercial-grade fire suppression and life safety solutions for all kinds of facilities, all around the world.

Office building next to a walkway and a garden

Industries

Rely on Johnson Controls to create healthier, more productive building environments that deliver energy savings, operational savings and sustainable solutions.

Closeup of an apartment building with vertical garden

Environment

See how we empower customers and communities to consume less energy and conserve resources — all over the world.